alert icon

Internet Explorer 8 or 9 is not supported by this website. Please use a more up to date browser.

Hide Message hide icon
Swagelok Southern California

Your Authorized Swagelok Sales and Service Center

WEBINAR: Fluid Systems for H2 Applications

swagelok hydrogen webinar

At this critical time in the emergence of hydrogen as an energy source, it’s as important as ever to show that hydrogen can be handled safely, efficiently, and cost-effectively. But that isn’t always easy.
Containing a small-molecule gas under pressure requires specialized knowledge. That is why clean energy professionals are increasingly bringing in hydrogen fluid system specialists to help them achieve first-time, long-term, leak-tight operation of their hydrogen systems.
If you could use help building and operating safer, more efficient, more profitable hydrogen systems, don’t miss this presentation by Chuck Hayes, Principal Applications Engineer for Clean Energy at Swagelok. He will explain how to engage effectively with technical advisors to:

  • Identify and estimate costs of existing hydrogen leaks in detailed reports
  • Categorize areas of concern by severity
  • Create an action plan to address them
  • Integrate best practices to avoid other issues

Whether you work for a hydrogen producer or a supporting OEM, please join us on May 18 to be sure you’re well-equipped to operate hydrogen systems that are properly designed, assembled, installed, and maintained

Led by Chuck Hayes, Principal Applications Engineer for Clean Energy at Swagelok, this presentation will discuss the critical considerations for fluid system components (tube fittings, valves, regulators, and hoses) used in hydrogen applications and systems. As a small-molecule gas, hydrogen can migrate through tiny crevices and diffuse into the materials designed to contain them. Also, high storage and dispensing pressures, as well as rapid thermal and pressure changes, are challenges for the processing of H2 as a fuel source. Specification of high-performing fluid system components designed for these challenging applications will help ensure the long-term, leak-tight operation of the system.

NOTE: This webinar is hosted by our friends at H2 View and will be a pre-recorded on-demand event. The webinar will go live at midnight (GMT) on March 28th.

register